This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2121: mux battery backup

Part Number: TPS2121


Tool/software:

I have a 24V supply from an external board that supplies power to a buck converter on my board to generate 5Volts and is connected to IN1 / pin 7.

I have a 5V backup supply from the same external board that is connected to IN2 / pin 2.

Using a resistor divider connected to the PR1 / pin 6 input, I would like to use the 24V supply to trigger the switch over from IN1 to IN2 when the 24V supply runs out of energy.