Other Parts Discussed in Thread: BQ27Z561-R2, BQ27426, BQ27427
Tool/software:
Hi All,
I have a question about the BQ27Z558.
Can it be used at 3.7V with a power consumption of about 1mA?
The battery capacity is 28mAh.
Can you tell me if it is possible to obtain the following parameters?
・Usage time
・Cycle count
・SOH
・SOC
・Cell voltage
・Cell current
Best Regards,
Ishiwata