Other Parts Discussed in Thread: TPS25751
Tool/software:
Description:
1. We use the TPS25730D (USB PD Controller).
2. A voltage divider is connected to the ADCIN1 input - 100k on LDO_3V3
and 5.1k on GND to program the min. voltage of 9V.
3. Only a 100k resistor on LDO_3V3
is connected to the ADCIN2 input to program the max. voltage of 20V.
4. Voltage dividers are connected to the ADCIN3 and ADCIN4 inputs
as in p. 2 to program the operating current of 1A and the max.
current of 3A.
5. Only a capacitor (bypass capacitance).
10 uF is connected to the VIN_3V3 input.
Question. Is it possible (and how) to change the operating voltage to 9V, 12V or 15V via I2C if the voltage source produces up to 20V.