Tool/software:
On the TPS22996H-Q1, is it allowed to keep VIN1 and VIN2 permanently connected to a power source (LiPo battery, 2.8-4.2V) while VBIAS can be unpowered temporarily (floating, disabled via load switch)? ON1/2 will be pulled low via pull-down resistor in this case and the outputs should of course be off. I also would like to run both channels in parallel as in the linked thread.
The datasheet states that VINx should be <= VBIAS, but will the device be damaged if this is not the case? What is the leakage current into VINx in with VBIAS=open, can there be a leakage current to VOUTx?
Thanks!