Tool/software:
Hi,
My design uses a BQ25155 to charge a single Li-Ion-battery and power a circuit with a microcontroller. This microcontroller will set the BQ to shipping mode via I2C once it needs to shut down. This mostly works, but in a few circuits I see a rapid loss of charge when it is switched off. In the most egregious case I measure 4.8 mA current from the battery even though most lines show zero voltage. The only parts where I measure any voltage (which is Vbat in all those cases) are the line to MR and VBAT on the BQ25155.Three other BQs in other circuits of the same design (out of 308 so far) also draw some current, but only between 0.22 and 0.5 mA.
Current starts to be drawn as soon as voltage is applied and the current rises with voltage. With 4.08 Volts at the battery, I measure 4.8 mA. When switched on, the circuit behaves as designed (with the almost 5 mA on top of the regular consumption, that is). The BQ communicates over I2C and delivers the 3.0 V requested by the controller. Battery charging also works properly. But when the circuit is switched off by sending the BQ via I2C the command to switch to shipping mode, the battery continues to be drained. I replaced the battery already and see the same behavior with the new battery, too.
Somewhere there must be an effective resistance of 833 Ω to GND. None of the resistors in the circuit has anything close to that. Also, an IR photo of the circuit (see below) shows a hot spot right where the BQ25155 sits.
The pins on the BQ are as follows:
MR and VBAT: 4.08 V from the almost fully charged battery
VIO, LS/LDO, LP are all interconnected and show 0 V
SCL, SDA are connected to VIO via their pullups. I can only measure them indirectly (at the pullups) where I see 0 V.
ADCIN, TS, GND are connected to ground, directly or via appropriate resistors
Has anyone seen this before? Is there a way to improve my circuit which makes the BQ stop to consume so much power in shipping mode? Again, three others out of a total volume of 308 circuits also draw some current in shipping mode, but less than 1 mA. The others are all doing fine, drawing a current below the range of my equipment. Are there known cases of shorts between single balls of the BGA which would explain this current?