This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25990: External I2C EEPROM Address Default

Part Number: TPS25990

Tool/software:

Hello,

I would like to use the TPS25990 with an external EEPROM for storing register configurations (or more specifically, so those configurations can be changed and saved more than twice).

The two EEPROM ICs specifically listed as compatible (24LC04 & 24AA04) both ignore the two address bits in the control byte:

Start Bit  Don't Care

   |         |

   S 1 0 1 0 x x B0 R/W ACK ...

               |

           Don't Care

However, the I2C EEPROM I have access to requires those bits to be deterministic. What two address bits does the TPS25990 utilize when communicating with the I2C EEPROM?

Thank you for the assistance!