This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM51231-Q1: If LM51231-Q1 can be used in master and slave mode?

Part Number: LM51231-Q1
Other Parts Discussed in Thread: LM5122

Tool/software:

Dear

Can I use two LM51231-Q1 in parallel to make sure high power output?  master and slave mode?

  • Hello Sun,

    Multiphase operation is not possible with the LM5123(1).

    Please either use 2pcs of the LM5122 controller, which has been designed for this purpose,
    or our new LM5125 which can drive two phases from a single controller.

    Best regards
    Harry