Other Parts Discussed in Thread: BQ24296
Tool/software:
I have a concern regarding the use of the BQ24295 charging IC in our custom circuit.
In our design, we are using both the SYS and PMID pins. The logic is set such that:
-
When the battery voltage is above 3.5V, the system runs from SYS.
-
When the battery voltage is below 3.5V, it switches to PMID.
This logic works well. However, when the system is running from PMID, we still observe a continuous input voltage (e.g., 4.3V or 3.6V) appearing at the SYS pin.
Since SYS is an output pin, I am concerned that this could negatively affect the IC—possibly by back-powering the output or causing internal conflict.
Can you please confirm if this behavior is safe, or if it could damage or interfere with the IC’s normal operation?