Tool/software:
Dear TI team,
I'm using the LM76005 in a 32–38V input to 5V/5A application, with a USB-C connector in parallel at the output used only for testing and debugging purposes. I have a few questions regarding this setup:
1. The datasheet doesn’t provide information about paralleling the LM76005 with another power source. How does the IC behave when 5V from USB-C is connected in parallel with the regulator’s output?
2. What happens if only USB-C power is present and the LM76005's VIN is left floating?
- Does reverse current flow through the IC (e.g., into the input capacitors)?
- Could this cause any issues for the IC?
- What about the case when VIN < VOUT?
3. Is it acceptable to leave both power sources connected in parallel, or would it be better to use an ideal diode (e.g. LM73100RPWR or others) to prevent potential backfeed or other issues?
Lastly, this is the design, could you review it?
/cfs-file/__key/communityserver-discussions-components-files/196/garpez.pdf
Thanks in advance for your help!
Gabriele Lotto