This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS55289: Shutdown effect on I2C bus

Part Number: TPS55289

Tool/software:

Hello. The specification of the TPS55289 states:

"When the EN/UVLO pin voltage is pulled below 0.4 V, the TPS55289 is in shutdown mode, and all functions are disabled. All internal registers are reset to default values"

 I have the impression that the I2C bus is not only inactive but also forced to ground. This is undesired as it blocks communication with other chips on the same bus.  Can you confirm this behavior?

Thanks

Jan