This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM20343: Transient on load current greater than 300mA

Part Number: LM20343


Tool/software:

Hello,

We have a transient that appears at the beginning of every clock cycle on the output once load current goes beyond 300mA with the amplitude of the transient increasing as the current is increased. Can I share additional test setup information, schematic and board layout via email?

Thanks,

Sinjon