Tool/software:
So, I try to connect this between a battery charger/battery (currently USB-PD-CHG-EVM from TI) and my load.
When I have the battery charger with 3S batteries connected to my load, it works absolutely fine on power up.
When I have my load switch (TPS22811EVM) connected in line, the load turns on for a while and then turns off and then tries to power on again.
It almost feels it couldnt handle the output slew requirements, so I removed the jumper from J15. That didnt help either.
J1 jumper is set to 5-6 as default.
Also now that I was playing with the jumpers, the EVM has completely stopped working even though there is a valid input.
So I have two problems---
1. How to get the load switch to function in my design (as I am designing it in)
2. Why is my EVM not working?