Tool/software:
Hi, TI
I would like to confirm ssettingus Rzx, Ra, Rb, and Rt.
(1)Increasing Rzx has improved Ithd.【figure1】
How much of an increase in Rz is reasonable? Are there any negative effects from increasing Rzx?
Also, when Rz=136k, Vout fluctuated between 390 and 400V for several tens of seconds after startup. There was no fluctuation when Rz=112k or less. What do you think is the cause of this?
(2)Is there any impact that Ra and Rb are one order of magnitude lower than in the data sheet?【figure2】
Ra=860k(date sheet 8.61MΩ), Rb=15k(date sheet 133kΩ)
Also, at what level should I adjust CINACX?
(3)How should I calculate Rt?
The data sheet shows equations (48) and (49), and KTH and KTL for Rt=133k are listed on page 7. Is it correct that KTH_min is 0.36 and KTL_min is 3? (I would like to confirm that it is correct to use the values for Rt=133k to calculate Rt.)
Also, I would like to know what parameters 133k and 4.825V in equations (48) and (49) are.
In addition, I believe that lowering Rt will extend the switching ON time, but what is the lower limit of Rt and what is the reason for it?
The background is that when Rt=100k, Vout=400V at AC=85, 115V, and 265V, but it dropped to 360V at AC=220V. I confirmed that when Rt=82kΩ, it becomes 400V at AC=220V. Therefore, I would like to determine whether this Rt=82k is a reasonable value.
Could you give me some advice?3326.UCC28064A.pdf