Tool/software:
Hi sir,
I am using bq34z100-r2 , sealed acid battery 12v 7Ah.What is the importance of the terminate voltage?
Design capacity - 7000mAh
Design voltage -> 5000mV by using the volt scale as 2
Number of cells -> 6
Design Energy -> 8400mWh
Tapper current ->100mA
Discharge current threshold -> 60mA
Charge current threshold -> 75mA
Quit current -> 40mA
I am not able to get the terminate voltage in my battery management studio instead I have got Cell terminate voltage.
Is both are the same?
I have kept the Cell terminate voltage to 2000mV.Whenever I start to discharge the battery up to 5000mV it will be discharging correctly. After when it reaches 5000mV it will drastically decreases to 0mV.Is it normal or if it wrong then what maybe the potential reasons for this drastic decrease in voltage ? what are the solutions for this problem?
Please reply as soon as possible.
Thank you
Tejas