This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5137-Q1: Please choose proper device for my customer.

Part Number: LM5137-Q1
Other Parts Discussed in Thread: LM5137F-Q1, , LM5137, LM5146, LM5145, LM5190

Tool/software:

Dear TI experts,

My customer considers DCDC buck controller for their next project. The specifications are as below ;

Topology : 4 phase buck converter (including Si MOSFET)

Input voltage : 51.2V (44 to 59)

Input current : 14.8A (12.9 to 17.2)

Output voltage : 12 ± 0.1V (9.0 to 14.6)

Output current : Max 60A for 4 phase

Power ratings : 720W

My customer found 4 parts as attached file below. Please choose best device for my customer.

It is okay that suggest other devices.

Compare-parametrics-202504081624_48-12V_Controller-20250408.xlsx

One more question, Could you check the RTM schedule of LM5137-Q1 and LM5137F-Q1?

Best regards,

Chase