This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Scott,
I don't think the LM5118 is appropriate for an application with this much input current (over 230 amps at 6V input). This is a tough specification given the low iput voltage, but I think a full wave topology would be the only way to go. Either a push-pull or a full bridge could handle the power better, but you would need a transformer which complicates the circuit. In my opinion though , that is the way to go.
Regards,
Ron Crews
Hi Ron,
I had a question regarding flexible voltage and amperage with a very similar conceptual design. I am using kenthal wire to create a resistance for a heating element. I am assuming I will be using a resistance of 2 to 3 ohms in order to achieve the highest wattage output possible with a battery with a continuous discharge rate of 240amps. The possible output I believe came to be near 800 watts and I am looking for a micro controller that will handle this load and if not how can I improve anything to make it do so.
Thanks,
Zack