Tool/software:
Hi Team,
Please provide the following operating state conversion efficiency of TPS631011
a.Vin 3.7 to Vout 3.4V
b.Vin 2.4 to Vout 3.4 V
Iout : 10uA, 20uA, 30uA.....to 100uA ,
A total of ten consecutive values
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Team,
Please provide the following operating state conversion efficiency of TPS631011
a.Vin 3.7 to Vout 3.4V
b.Vin 2.4 to Vout 3.4 V
Iout : 10uA, 20uA, 30uA.....to 100uA ,
A total of ten consecutive values
Thanks
Hi Tao,
It will take a week for the EVM to arrive.
Please set aside time for testing
Thanks
Hi Allen,
Please expect i can give you the results next week.
Regards
Tao
Hi Allen,
Please refer the data below.
Vin | Iin | Vout | Iout | EFF |
3.703 | 103.2 | 3.3 | 100 | 0.863536 |
3.704 | 94 | 3.3 | 90 | 0.853017 |
3.705 | 84.3 | 3.3 | 80 | 0.845256 |
3.706 | 74.8 | 3.3 | 70 | 0.833307 |
3.707 | 65 | 3.3 | 60 | 0.82173 |
3.708 | 56 | 3.3 | 50 | 0.794614 |
3.71 | 46.2 | 3.3 | 40 | 0.770119 |
3.711 | 36.8 | 3.3 | 30 | 0.724931 |
3.712 | 27.4 | 3.3 | 20 | 0.648911 |
3.713 | 17.8 | 3.3 | 10 | 0.499309 |
2.417 | 26.8 | 3.31 | 10 | 0.510995 |
2.415 | 41.8 | 3.31 | 20 | 0.65579 |
2.413 | 56.5 | 3.31 | 30 | 0.728356 |
2.411 | 71.3 | 3.31 | 40 | 0.770196 |
2.409 | 86.3 | 3.31 | 50 | 0.796068 |
2.407 | 101.3 | 3.31 | 60 | 0.814505 |
2.405 | 116.1 | 3.31 | 70 | 0.82981 |
2.404 | 130.9 | 3.31 | 80 | 0.84148 |
2.402 | 145.6 | 3.31 | 90 | 0.851797 |
2.4 | 160.6 | 3.31 | 100 | 0.858759 |
Regards
Tao