This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90160A: Queries Regarding UCD90160ARGCR Configuration and Flashing via I2C

Part Number: UCD90160A

Tool/software:

Hi,

I am using the UCD90160ARGCR as a power sequencer in a custom board design, and I have a few queries regarding its configuration and flashing process:

  1. Our custom board uses the UCD90160A along with a host processor that communicates via I²C using the PMBus protocol.

    • Can I configure and flash the UCD90160A using the I²C interface?

    • Also, is any additional hardware required to configure or operate the device using I²C/PMBus?