Tool/software:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Tomas,
Thanks for reaching out.
It looks like the attachments did not send. Could you please resend them so I can review the waveforms?
Best regards,
Alec
Hi Alec,
I really can't send attachments, I don't know what to do with it. Because the form and insert only allows me to send the URL of the image, but I don't have it shared anywhere.
So how do I send images from the oscilloscope?
The only thing I can send is a print screen form, that works
Thanks and have a nice day.
TK
Hi Tomas,
Thanks for reaching out.
Try copying and pasting the image into the field. Alternatively, there should be an option to upload the file directly:
Best regards,
Alec
360mA load
--------------------------------------------------------------------
Free load 1
Free load 2
Free load 3
Hi Tomas,
Significant voltage drops are not expected in low load conditions.
Can you please share waveforms of VBAT, VSYS, SW, and PMID in parallel to see if the boost output is being impacted along the power source path? Additionally, can you please share the register values when un-loaded, when 360mA load, and after the 400mA load collapse?
Best Regards,
Juan Ospina