This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with bq24072 Li-ion charger - Everything seems OK, except no charging

Other Parts Discussed in Thread: BQ24072, BQ24072T

Hi

I am trying to debug non working of bq24072 battery charger with DPPM, but stuck at a point, the details are as:

Vin = 5.2V, EN2 = Vin, EN1 = Vss = TD = CE, Rtmr = 47k, Riset = 820E, Rilim = 2k2, 4.7uF ceramic across battery & 10K NTC/Resistance on TS

PGOOD is always Active, and CHG is active when battery is connected. When battery not connected, Vbat shows slow square wave as per datasheet. Vout = Vbat + 200mV when battery connected else it is 4.4V

Li-ion battery voltage is 3.1V and 3.8V and none of these are getting charged (Based on measured current to the battery is zero)

All signals, symptom and indicators seems OK, but battery is not getting charged (zero charge current), what could be the reason?

 

Thanks in advance.

Regards

Pavan