Other Parts Discussed in Thread: TPS610333
Tool/software:
Hi All,
Im planning to use the TPS61092 chip in order to convert:
Vin that could be from 3.7-4.2 Volt when the system is in battery mode
Vin at 5V when in wall adapter 5V mode
Vin is the output of a power path circuit and could be provided by lipo or 5V fixed.
Attached there is my circuit.
Vout : should be 5V max 2A
L1: CDRH103RNP6R8NCB
FB pin: floating
LB1: R33=1.87Mohm, R32=340Kohm
C26 = TPSD107M010R0050 - 100uf

Can you validate the schematic? in particular: will do it work with 5V input? Could be FB pin left floating ?
Thanks a lot
Nicola