Tool/software:
Hi,
We are using LM5109B for our motor driving application for driving the H-Bridge circuit given below.


We see a strange issue, We've provided a dead time of 2.5uS between the HI and LI PWM Inputs, that is the maximum supported by the Motor driver chip that we are using. But when we look at the HO and LO waveforms, the HO signal stays high even after the HI pin is low and it stays high until the LO starts to rise. See the below waveform,

Yellow- HO w.r.t. GND
Pink- LO
Cyan- HI
Green-LI
We are using 48V for powering the H-Bridge.
Because of this we see a ringing on the rising edge of LO and similar ringing is observed on the other voltages and digital signals on the board.
Could you please help us find out the root cause of this problem?