Tool/software:
I have the UCC25660EVM-064 module. The module has UCC256601 integration. But I don't want to use the HV pin and Vcc Aux voltage. In the datasheet, it says to replace it with the UCC256603 integration as can be seen in the picture below. UCC256603 is not available for sale. How can I make the HV pin disable in the UCC256601 integration in UCC25660EVM-064 module? How can I supply it with external VCC in UCC25660EVM-064 module?