Tool/software:
we need to details of schottky diode, if we can use schotky diode then my output supply voltage is change 5v to 7v output please suggest solution
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I do not understand your question. Are you referring to the Schottky diode used for reverse current protection for this device? You need a Schottky diode with a low forward drop because you want to make sure the reverse current is flowing through the external diode rather than the parasitic body diode of the pass FET. If the Schottky has a lower forward drop then the body diode, it will activate first.
Sizing the forward current of the Schottky will depend on the nature of the reverse current situation. Are you expecting an indefinite short from VOUT to VIN (which is being tied to GND)? Or is VOUT shorted to VIN which is going high impedance? It can be helpful to try to measure the current in this scenario to determine how big of Schottky you need. If it's a momentary short, you may be able to find an appropriate Schottky diode that can handle the associated surge current.
In general, you can assume parasitic body diodes to turn on around ~0.6V - 0.7V. Try to find a Schottky with a lower forward voltage across temperature, current and any other relevant conditions
Regards
Ishaan
It is not possible to debug this without a schematic. Please share a schematic showing your schottky diode and 1N4148 device connections. Please also share scope waveforms which show 'misbehaving' output voltage