Other Parts Discussed in Thread: BQ25756EVM, , BQ25750EVM, BQ25756
Tool/software:
Hi, I am trying to demonstrate the following setup as shown in the image:
One TPS26750EVM with BQ25756EVM as a source to provide 24V 5A power. The power on the source comes from HV_SYS which is connected to a bench power supply.
One TPS26750EVM on the other side acts as a sink, sinking 24V 5A power. An EPR USB-C cable is used to connect them together.
The issues I am seeing are:
1) When HV_SYS = 5V, VBUS on source J4 and sink J4 were measured to be 3V. Doesn't look right to me.
2) When HV_SYS = 24V (or any voltage above 5V), the PP_EN and VBUS LEDs on the source flash at 1Hz rate, basically the VBUS output toggles between 0V and 5V every second. Seems like the system is constantly resetting.
I think I have programmed the boards correctly.
Would really appreciate any FAE support here.
Thanks!