This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS552892: Maximum output current verification

Part Number: TPS552892


Tool/software:

Hi,

I want to use TPS552892 for the following design requirements:

Vin = 11V to 20V
Vout = 12V
max. Iout = 6A

This seems fine because the min. average inductor current limit is 7A.
But the Webench says, "Your preferred device does not work with the inputs you selected."

Could you please check this?