This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ51003: Datasheet, error in Typical applications schematics

Part Number: BQ51003
Other Parts Discussed in Thread: TIDA-00318,

Tool/software:

Hi! Was checking out the schematics of the TIDA-00318 reference designs, and it caught my eye that there is a 20K resistors between RECT and FOD of BQ51003.

I checked the typical applications section in the BQ51003's datasheet (Figures 32 and 38) and that resistor is labeled Ros2. However, section 9.2.1.2.5 mentions "Default values of 20 kΩ for Ros1 (RECT to FOD). Ros2 (OUT to FOD) remains open. Hence the resistor in TIDA-00318 is Ros1 and the schematics in the typical applications section are misleading.