Other Parts Discussed in Thread: LM5156, LM5122, LM51561
Tool/software:
Hi TI experts,
I used LM5022 in my old projects for isolated flyback design, the input is 9-60V and output is 12V/2A.
But LM5022 seems simple for protection function and the primary OCP is hiccup, but not latch off.
Can you advise alternative controller for isolated flyback design with below features?
1. Can support wide input voltage range 9-60V
2. Can replace LM5022 with minor external component (transformer/FET/Rsense,etc) changes to existing design
3. With more protection function like OC/OV (Latch off mode is preferred)
4. Can be used for secondary Synchronous rectification to improve the conversion efficiency
Please kindly advise.
Neo