This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS922055DRRREVM: Determination of Led driver Vout

Part Number: TPS922055DRRREVM

Tool/software:

Hi,

I did some test with tps922055evm and somethings confused my head. When supply voltage is 28V and no load condition, measurement of output voltage is about 26V. In load condition, my led forward voltage is 3.4V and 7 series. So ı measure output voltage and saw 23.8V in %100duty cycle. There is no problem so far. But when ı changed the load (3V x 5 led), Vout still 23.8V and my led blow. First question, why ı did measure 26V in first place? Second, Why didn't the output voltage change automatically when I changed the load?Because the datasheet says "VOUT is the sum of the voltage across LED load". Third question is how can ı be sure my led driver is working in cc mode? 

Thank you for feedback.