This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5190: constant current supply

Part Number: LM5190

Tool/software:

Hello,

Is there an IC to design a constant current supply with the following parameters:

  • Input: 10-13VDC (50Watt max)
  • output 4A constant current (steps up from 1A to 4A preferable)

I found the LM5190, but to complex!

Best Regards,

Piet

  • Hello Piet 

    In WVB team, I think LM5190 is the device capable of CC regulation with integrated the CC regulation loop. If your maximum input is only 13V, then please contact MVB/LVB team and check if any better device. 

    -EL