Tool/software:
Dear Team,
using the TPS25751 in a docking-station where it should be able to source up to 100W to the connected notebook. The external power-supply of the dock is not e.g. a power supply unit with a fixed output voltage which provides >100W but it will be a USB-C Power adapter providing various voltage/current settings and maybe it provides only 65W or less. Is there a possibility to tell the TPS25751 what is the maximum available voltage/current so it can adjust the transmitted source capabilities (PDOs)? Is there a sink(-only) PD-controller available which can be used for the external power input which can correspond with the TPS25751?
Thank you
Regards
Norbert