Other Parts Discussed in Thread: LMR66430, TLVM14406, TLVM23625
Tool/software:
Hello team,
I'm creating the design with the condition, Vin:24V / Vout: 2.3V / Iout :2A.
If I use LM62460, Webench is warning about minimum On time operation. So, if I reduced the switching frequency, the design updated failed due to low phase margin.
webench.ti.com/.../125

However, if I use LMR66430, there is no minimum on-time operation even 2.2MHz switching frequency. On time spec is similar for LM62460 and LMR62460.
So, I'm not understanding why LM62460 cannot satisfy the specification.
webench.ti.com/.../124
Also, if possible, you can suggest the right solution for this condition. The customer is looking for the solution which has high efficient and good thermal performance
Best Regards,
Austin