Tool/software:
Hi,
with TPS55287 i was aiming for 2.14MHz fsw, but spread spectrum dithering would introduce a triangular waveform which modulates the oscillator frequency by ±7% of the nominal frequency. So i would end up with 1.99MHz-2.29MHz, and would be above the max allowed 2.2MHz.
Still possible or should i aim for a lower nominal switching frequency if i want to use spread spectrum dithering?
also the the EVM uses ~700Hz dithering frequency at 400kHz fsw, should i also aim for 700Hz dithering frequency with a fsw > 2Mhz or is a higher dithering frequency better?
Thank you in advance