This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25792: REGN pin fails whenever battery is connected to the charging board

Part Number: BQ25792

Tool/software:

Hello sir I am using the BQ25792 ic for charging 2s lithium battery(8.4V)  I created schematic as per the datasheet template but when comes to working whenever i connect   the lithium battery to the charging  board my REGN  pin becomes short . I used RPS to supply voltage for vsupply pin of ic i gave 5v 1A initially when there is no load i viewed my ic consumed some mw power and i checked the voltage at the regn pin which is found to be 5v but when i connect battery to the system i face this issue and  i placed a 4.7uf capacitor with 25v rating  and i placed a 6k resistor in prog pin ( 3k series combination) as i do not have 6.04k resistor  and i used a shunt resistor 0.01ohms in charging side to check the charging current , i placed 100ohms resistor in series with BATP pin and Battery i just want to know the reason for this fault in regn and can u mention what are the possible reason for this short. 

Note: i did not use sys pin and i disabled TS with voltage divider