Hi all,
i have some questions to the MPPT of the BQ25504:
On Vin_DC i have a solar cell with a open circuit voltage of 4V.
When the booster is aktiv, the voltage on the input pin is 0.35V.
I think, that the generated current of the solar cell is to small.
But the solar modul is a big modul with enough power.
I think the MPPT is incorrect and the load on the BQ25504 is to big.
Can you agree this?
Thanks