Tool/software:
Hello,
We are using the BQ24298 as a battery charger and also for OTG boost conversion. We are seeing all functions working as expected in ideal case scenarios, meaning, the battery charging, auto-cut-off, dynamic power path management and Boost Conversion, etc everything works fine and our software senses low charge and then shuts down the system.
The problem is seen while trying different batteries that if the software fails to turn down the system on low battery conditions for any reasons (faulty battery or improper charge calculations), then the BQ24298 goes on a mission to staying alive and keeping the voltage Vsys ON and in doing so is getting martyred (damaged) as I would like to believe.
We attempted to mitigate this by setting a higher SYSMIN threshold, and stopping my soldier (BQ24298) from getting into an uncalled war (exerting too much), but this hasn’t resolved the issue.
This has now happened in almost 3 prototypes and we need some guidance into solving this. Are there any particular settings that can be applied or an external protection that we should be using with BQ24298 to cut-off. Please point us in to right direction.
Regards,
Arif Gilani