Other Parts Discussed in Thread: UCC28704, UCC28722
Tool/software:
I would like to use the UCC28704EVM-724 design as a starting point for a high input voltage, isolated, DC-DC converter. Input voltage range = 200Vdc - 1200Vdc (This is ideal, 450Vdc-900Vdc may be ok), output voltage = 24V, max output current = 1.87A. Aside from the obvious component voltage/current rating modifications what other modifications would need to be made to the UCC28704EVM-724 design to meet this higher input voltage requirement?