Tool/software:
I would like to ask about the TPS65131 component. The measured FBP voltage is not within the range specified in the datasheet. One is around 1.36V and the other is 1.42V. The Vref voltage is 1.176V, which is also out of the range specified in the datasheet. This will cause the set output voltage to be incorrect. Could you please help me figure out the reason for this? If there is any problem with the schematic diagram, please check it for me. Thank you!