Other Parts Discussed in Thread: BQ25756, BQ25750, BQ25751
Tool/software:
Hi,
In the datasheet, in section 6.3 Recommended Operating Condtions, some values are indicated which I would like to understand the reasoning behind them.
For Cin, a minimum of 80uF is recommended. Where does this come from? For this component sizing you have to consider the input voltage ripple if working as buck with power flow towards the battery and the output voltage ripple as well as implications in the regulation if working as a boost with power flowing from the battery. Beyond that, where does the 80uF come from? What is the impact of having, say, 10uF?
Similar with the inductor, why should the inductance be constrained between 2 and 15uH? What are the implications in case this values are not honored?
I would like to use a 22uH inductor and a 10uF capacitor, approximately.
Regards