This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6593-Q1: TPS6593-Q1, To gain a detailed understanding of the RTC wake-up feature

Part Number: TPS6593-Q1

Tool/software:

Hello Forum,

Could you connect with me the device expert for the following part code TPS6593-Q1.

I would like to gain a detailed understanding of the RTC wake-up feature.

Our Application: We planned to replace the individual Buck converters to single PMIC for our Development Boards.

About Mindgrove: MIndgrove is a fabless design company and successfully taped out our First SoC and is currently preparing the development and application-specific boards.

PMIC used to Power down our Mindgrove Application board wrt the enable signal (1.8V) received from the Mindgrove Soc.

For  power-up the Mindgrove Application Board in 2 modes. ( both modes implemented in simultaneously)

* Auto Mode: Once Mindgrove App board needs to wake up after a power down event, using either a RTC or timer to control the wake up time

Example sequence: Application Board--> Power Down Signal from SoC--> PMIC disable the rails--> Interrupt generate from RTC ( In-build with PMIC)--> PMIC enable the rails.

*Bypass Mode: When Mindgrove App board is power Down, it need to Power up (wake-up ) the board wrt the External switches (ex: Touch display or Push button)

Sequence: Application Board--> Power Down Signal from SoC --> PMIC disable the rails--> Interrupt generate from  Push button ( external one)--> PMIC enable the rails.

Thanks,

Ismail P

ismail@mindgrovetech.in

Mindgrove technologies

  • Thank you for your inquiry. US and Europe TI offices are closed on April 18th. You will receive a response early next week. Thank you for your patience!

    Regards,

    Katie

  • Hello Katie,

    Awaiting for your team responses.

    Thanks

    Ismail P

  • Hello Ismail,

    Thank you taking the time to look at the PMIC and it's features.

    The RTC needs the crystal portion of the PMIC to be populated to use the RTC feature.

    The RTC is considered an ON Event which can be tied to several hardware triggers, the snippets below from the datasheet will show the details.

    It should be noted that the PMIC is completely programmable from a state machine, so what the On Event does is dependent on the programming of the PMIC, which for Mindgrove with their SoC would be attractive as there can be split power domains, partial sleep mode, deep sleep with RTC wake up, etc...

    If you have questions about defining the programming for such a PMIC, please do ask.

    From the datasheet of the TPS6593-Q1:

    An example for a PMIC that already has it's state machine defined, note (TPS6594133A is a sister product):

    Example sequence: Application Board--> Power Down Signal from SoC--> PMIC disable the rails--> Interrupt generate from RTC ( In-build with PMIC)--> PMIC enable the rails.

    *Bypass Mode: When Mindgrove App board is power Down, it need to Power up (wake-up ) the board wrt the External switches (ex: Touch display or Push button)

    Sequence: Application Board--> Power Down Signal from SoC --> PMIC disable the rails--> Interrupt generate from  Push button ( external one)--> PMIC enable the rails.

    This can be achieve from a series of different triggers, but the most important question is the expectation of safety features and would the preregulator be turned off during this Bypass Mode. The expectation from any of the wake-up is that the regulator is up and in a known good state otherwise the power up would encounter errors, otherwise this is possible.

    Best Regards,

    Nicholas McNamara

  • Hello Nicholas,
    Could you please share the meeting link for the next working day in IST? For your reference, my available hours are between 10:00 AM to 7:00 PM IST, or between 9:00 PM to 10:20 PM IST. I have a few more questions to clarify regarding the manual (User guide & GUI user guide) and the implementation on our development board.

    Also, could you please share a sample program to help me understand it more easily?

    Thanks,

    Ismail P

  • Hi Ismail,

    Do you have a local TI field applications or sales contact? They may be more available at the time you are talking about and could speak to you in more private format than the public forum if you are wanting to get more into details of your application/development. 

    Regards,

    Katie