This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61165: This is a question about PWM control.

Part Number: TPS61165


Tool/software:

The frequency range that can be set from the data sheet is 5kHz to 100kHz.

Is it possible to set the duty ratio to 1% to 100% throughout this frequency range?
(Does the duty ratio that can be set change depending on the frequency within this frequency range?)