This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28950: Regarding the design constants for the current transformer.

Part Number: UCC28950

Tool/software:

Hi team,

My customer is considering using the UCC28950.

I have a question regarding the design constants for the current transformer in the current detection line.

According to the WEBENCH design data, a current transformer with Lp = 20 mH is recommended, but I don't know the inductance value of Ls.

Should I use a transformer with Lp = 20 mH and Ls = 200 µH based on the following WEBENCH design data?

Lp = 20.0 mH

Rp = 891.633 mOhm

Leakage_L = 20.0 µH

Ns1toNp = 100.0

Rs1 = 4.8 mOhms

Best regards,