This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC25600: Full bridge LLC Design 60VDC @ 25A

Part Number: UCC25600
Other Parts Discussed in Thread: UCD3138, UCC28950

Tool/software:

I am to start working on a dc dc converter, following are my requirements.

Vin; 26V, Range:20-32V

Vout: 60V, 25A, 1500W, Isolated, conduction cooling, fan-less design

I am thinking of doing it with LLC converter, will it be good approach and the IC mentioned is capable full bridge LLC configuration?

I am open to recommendations on design approach.

Thanks