This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMICLOADBOARDEVM: TPS6594_Q1 Low temperature failure

Part Number: PMICLOADBOARDEVM

Tool/software:

Dear TI Support,

Follow the datasheet, the device temperature grade :-40°C to +125°C.

If the ambient temperature is lower than -40°C, what abnormal failure will TPS6594_Q1 have? Will it cause the system to shut down all digital outputs, external voltage rails, and monitors and enter a safe recovery state after a self-test exception?

When we start the low temperature pressure measurement, we find there are occasional PMIC failures. the PIN status follow:

EN_DRV              LOW
GPIO9 PGOOD   LOW
GPIO2                 LOW
nRSTOUT           LOW

When the temperature returns to around 20°, the problem will be fixed. Can we determine that the PMIC is abnormal based on these PIN states? What is the minimum operating temperature of this PMIC?