This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24072T: System operation during batterry charging

Part Number: BQ24072T

Tool/software:

I am considering using the BQ2407xT to operate a system while charging the battery.

The system consumes an average current of about 12mA when powered, and a peak current of about 1A when the processor starts up.

I am thinking of connecting the battery to the BAT terminal and powering the system from the OUT terminal, but since the peak current at startup is large,

I am concerned that this will not be a problem. Is it possible to create such a system with the BQ2407xT?