This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24640: Our put voltage issue

Part Number: BQ24640

Tool/software:

Hi,

1. Input Voltage = 24V , Output Voltage = 12V , I charge = 3A , We have used supercapacitors 5x25F/2.7V each connected in series

Observation: We are getting output voltage 5.82V at super cap/sense resistor and feedback voltage is 1V,Based on calculations(equation 1) we have set lower feedback resistor value is 10K and upper feedback resistor value is 47K

we are not getting output voltage 12V,So please suggest solution for this problem. please find the below attached schematic  

Regards,

Sreehari.