Tool/software:
I am to start working on a dc dc converter, following are my requirements.
Vin; 26V, Range:20-32V
Vout: 60V, 25A, 1500W, Isolated, conduction cooling, fan-less design
Question is if it's possible to achieve a high eff psfb design given my specifications. I haven't found any ref design or paper close to what I want. Webbench generated a very non practical schematic which is not possible for e.g. 300mF input capacitance. The main issue however is leakage inductance, even SLUC222 tell me to have a Lk of -4uH. So, I am want to know what approach to design should I follow?