This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5137F-Q1: Average model of LM5137 in SIMPLIS

Part Number: LM5137F-Q1
Other Parts Discussed in Thread: LM5137

Tool/software:

Is there any average/AC simulation model of LM5137 in SIMPLIS?

  • Hi Brian,

    Unlike PSPICE, the same file in SIMPLIS does both Transient and AC modeling.

    Here is an introductory file that simultaneously models load transient response and bode plot (this is based on the 5V and 3.3V, 20A, 440kHz EVM):

    https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/196/LM5137-5V-and-3.3Vout-20A-440kHz-dual-output.sxsch

    Regards,

    Tim