Other Parts Discussed in Thread: BQ34Z100
Tool/software:
Hi There,
I need a fuel gauge IC for accurate SOC and health estimation for a single NiMH cell, 504-6219 from RS with a nominal voltage of 1.2V. Is the BQ34Z100-R2 adequate for this purpose? I can see that it does single cells but I was wondering if this is only applicable for Li-Ion, as the cell voltage for these is much higher at 3.6V. I will have a boost converter to provide a 3V3 rail to power the BQ34Z100-R2.Is there anything else I need to consider for my case to use the BQ34Z100-R2?
Thanks in advance :)