This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28740: Inquiry about IC enable & disable

Part Number: UCC28740

Tool/software:

Hello,

I’m planning to design an input series flyback converter using the UCC28740.
During the design, I want the converter to turn on at a specific input voltage and off at a lower voltage.

For example, I want the converter to turn on at 250V input and turn off at 200V.
Is it possible to implement such a feature with the UCC28740?
Or is there another controller IC that supports this functionality?